This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS16F95QML-SP: Worst Case Power Consumption Calculations

Part Number: DS16F95QML-SP
Other Parts Discussed in Thread: DS16F95QML

I am looking at making a absolute worst case analysis for this part, and I am curious if the output from the driver also influences the power consumption of the DS16F95QML. My system currently has 1 DS16F95QML driver connected to 3 DS16F95QML receivers. Do I need additional calculations on top of the Icc = 28mA when the receiver and driver are turned on? My impression is that is essentially the quiescent current. Please let me know if this information is sufficient or if more detail is needed.

Thanks!

Ben