Part Number: PCA9306
Other Parts Discussed in Thread: SN74LVC2G66
Can VREF1 = VREF2 = 3.3V? Just to use the PCA9306 to isolate one I2C bus from another.
Related: Can VREF2 = 0V when VREF1 = 3.3V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCA9306
Other Parts Discussed in Thread: SN74LVC2G66
Can VREF1 = VREF2 = 3.3V? Just to use the PCA9306 to isolate one I2C bus from another.
Related: Can VREF2 = 0V when VREF1 = 3.3V?
Yes, but you could replace it with two wires.
When VREF1 = 0 V, a current will leak from VREF2 to VREF1. But when VREF2 = 0 V, EN also is 0 V, and the I/Os are disconnected.
Inderjit,
Clemens is correct. If your supplies are equal to each other you can use the device in a switch configuration:

Best,
Chris