This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI84: Flicker and screen shift when refreshing by mouse

Part Number: SN65DSI84

SN65DSI84 working as a bridge chip connects the mipi to dual LVDS LCD.

Issue: Flicker and screen shift when refreshing by mouse 

No movement from mouse, screen as below.

Refreshing by mouse, screen as below flicker and screen shift occur.

 MIPI output: RGB888, 110 MHz

LVDS: 10 channels

Screen: 8-bit LCD panel resolution 1280 * 1024

SN65DSI84 0x12: 0x16 110-115MHZ

SN65DSI84 other register configuration as below:

0x09, 0x00
0x0A, 0x01
0x0B, 0x18
0x0D, 0x00
0x10, 0x26
0x11, 0x00
0x12, 0x16
0x13, 0x00
0x18, 0x6c
0x19, 0x00
0x1A, 0x03
0x1B, 0x00
0x20, 0x00

0x21, 0x05
0x22, 0x00
0x23, 0x00
0x24, 0x00
0x25, 0x04
0x26, 0x00
0x27, 0x00
0x28, 0xb7
0x29, 0x00
0x2A, 0x00
0x2B, 0x00
0x2C, 0x00
0x2D, 0x00
0x2E, 0x00
0x2F, 0x00
0x30, 0x07
0x31, 0x00
0x32, 0x00
0x33, 0x00
0x34, 0x01
0x35, 0x00
0x36, 0x00
0x37, 0x00
0x38, 0x00
0x39, 0x00
0x3A, 0x00
0x3B, 0x00
0x3C, 0x00
0x3D, 0x00
0x3E, 0x00
0x0D, 0x01
0x09, 0x00

Could you help check the register configurations and provide suggestion for troubleshooting? Thanks.

Best Regards,

Tess Chen