Part Number: SN65HVD3086E
Other Parts Discussed in Thread: LM22675, LM25011
Dear Parker
We did further tests and would like to share our results. Request your advice.
1) During further tests, we find when the RS422 signals and DC_24V are separated and connected using separate cables, this problem does not occur. The RS422 signals is OK with cable length of 200 to 300 meters, when DC_24V is not present on the same cable.
2) On our board have used DC-DC converter IC LM25011MYX/NOPB 9V-30V to 5.00V @ 1A. We had followed the design as shown here https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=80D4213D6E367940
3) We tested with a older generation product that uses a different DC-DC converter LM22675. This problem is not seen.
4) Our device connect using CAT5/CAT6 cable to the remote master unit. This is the RJ45 cable connection signal & pin details.
| Pin# | Signal | RJ45 Cable |
| 1 | Tx+ | White Green |
| 2 | Tx- | Green |
| 3 | Rx+ | White Orange |
| 4 | DC_24V | Blue |
| 5 | DC_24V | White Blue |
| 6 | Rx- | Orange |
| 7 | GND | White Brown |
| 8 | GND | Brown |
Regards
Sandra