Part Number: DS90UH940N-Q1
Hello,
According to DS90UH940N-Q1 data sheet setting RX_LOCK_MODE = 1, will result in RX-LOCK assert when device is linked to a Serializer even if
active video is not being sent.
Here does it mean only the General_Status Register (Address = 1Ch) Bit 0 will be set when device is linked to a Serializer even if
active video is not being sent, or the Both the register 1C Bit 0 and the Hardware LOCK pin will also be set?
Are the register 1C Bit0 and hardware pin LOCK (PIN 1 of the IC) in sync?
Best regards,
Prasad.