Part Number: TCAN1462-Q1
please help suggest suitable PN.
the customer need:
In addition the CAN transceiver shall be based on NXP solution (as optional), to be compliant to cybersecurity requirements.
The NXP transceivers shall have the following features:
Configuration of Stinger can be included as part of ECU software block;
Protection by standard Secure Flash & Secure Boot;
Specific CAN messages to change the NXP Configuration in development phase countermeasures to avoid the downgrade;
Configuration protected by means of digital signature.
Note: details about NXP transceivers shall be defined during development
thanks!