This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] DS90UH949-Q1: Disable HDCP to work with UB Deserializer

Part Number: DS90UH949-Q1


Hello,

My customer would like to use DS90UH949-Q1 devices in place of the DS90UB949A-Q1 to keep production running. In reviewing the details they have the following questions.

  1. Can the HDCP function be disabled? If so, how is this done?
  2. Is the UH949 compatible and is it still under warranty when connected to a UB deserializer in production?
  3. Can you confirm the devices are P2P with no HW changes?

Thank you,

Alex