This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550: VSUP specifiation and bit rate configuration

Genius 17965 points

Part Number: TCAN4550

Hello,

 

My customer has 2 questions for TCAN4550

 

1.

According to the datasheets, TCAN4550(non-Q1) supports up to only 24V VSUP while TCAN4550-Q1 supports up to 30V VSUP.

Is this 24V VSUP specification for non-Q1 version correct? They want to use it with 24V +- 10% power supply and confirm this specification just in case.

2.

TCAN4550-Q1 supports up to 8Mbps.

Is it possible to configure 5Mbps?

 

Regards,

Oba