This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD251: P2P alternative for the SN65HVD251 parts

Part Number: SN65HVD251


Hello experts,

I would like to find 2p2 alternatives for the SN65HVD251DR (part of the SN65HVD251 family).
I'd note that even out of stock alternatives are ok Slight smile

Thanks,
Vlad

  • Hi Vlad,

    If the slope control feature of SN65HVD251 is not being used, the TCAN1044A would be a good pin-2-pin alternative for this device. The TCAN1044A uses our newest manufacturing process and will be the best choice for longer-term supply when talking about 8-pin CAN transceivers. Note that the 'V' version of TCAN1044A should not be used as the pin 5 function will conflict with the Vref function of SN65HVD251. The non-V TCAN1044A has a NC for pin 5, so it is compatible with such a pinout. 

    Let me know if you have any more questions.

    Regards,
    Eric Schott