Part Number: DP83867CS
Hello,
Our customer plans to utilize three power supply configuration.
In this case external 1.8V regulator output is shared to VDDA1P8 and VDDIO with specified bypass capacitors located nearby pins.
What is acceptable 1.8V regulator's output voltage variation?
We can see on the datasheet, there is Recommended Operating Conditions for VDDA1P8 as below.
VDDA1P8 1.71(min) 1.8(typ) 1.89V(max), Also VDDIO has same specification.
So, if external regulator's Load regulation is within this voltage range DP83867 can work fine?
Regards,
Mochizuki