Part Number: TLIN1021A-Q1
Hello team,
TLIN1021A-Q1 has the function which can let us know which wake source get the LIN to wake.

The weak pull down is 350kOhm shown below, and hard pull-down shown below as FET respectively correct?

And these characteristics are shown below, right?

Question
1. Hard pull down characteristics is specified as ITXD(WAKE) in case TXD=1V.
Does this mean the pull down resistance in case local wake is the wake up source is from 125Ohm(=1V/8mA) to 769Ohm (=1V/1.3mA)?
2. When we would like to recognize wake up feature what circuit is recommended?
Pull up the TXD with approx. 10kOhm resistor or something like this?
Thanks.
Regards,
Hirata