Part Number: DS90UB935-Q1
Hi Expert,
I find below pic from 935 datasheet. Is there anything wrong for these two bits? Thanks.

BR,
Elec Cheng
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB935-Q1
Hi Expert,
I find below pic from 935 datasheet. Is there anything wrong for these two bits? Thanks.

BR,
Elec Cheng
Hi Expert,
Add one more question. how can 960 tell it's 935 or 953 connected? Thanks.
BR,
Elec Cheng
Hello Elec,
No, this is actually correct. 953 and 935 have the exact same reg map. There is no way to differentiate between the two in SW. The only method we could recommend is that during the schematic design phase, the customer could use the IDX pin to set a certain address for modules using 953 and then a different address for modules using 935. Then through SW the device I2C address can be read and the customer can know which device is populated
Best Regards,
Casey