Part Number: DP83TD510E
Hi,
I have a question concerning the use of the differential transmit and receive pair signals.
According to the pin layout, there are four pins for the transmit and receive signals, i.e. Tx+, Tx-, Rx+ and Rx-.
So far, in order to be compatible with single-pair cables, I have only seen that these signals are reduced to a single pair, namely TRD_P and TRD_N using the termination circuits, e.g. as shown in the application section of the datasheet.
However, is it possible to use Tx+, Tx-, Rx+ and Rx- directly in a two-pair configuration, as shown in the figure below, with the according termination and component values?

And would this also allow full-duplex data transfer at 10 Mbit/s? I.e. would the transceiver work with a 10BASE-T PHY?
Also, should GPIO2/STRAP10 then also be pulled down, since a 50 Ohm termination is being used in this configuration?
Thank you in advance for your response!