This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848T: AN0/AN1 strap configuration

Part Number: DP83848T

Hello,

 

My customer has a question for the strap configuration of AN0/AN1(advertised mode).

AN1 pin is available on only J/K devices and not available on H/M/T devices.

For these H/M/T devices, how to configure this advertised mode?

 

Regards,

Oba

  • Hi Oba,

    The way I understand the following statement is:

    Since pin 21 is internally pulled up, and since the default on the DP83848x, then I assume you can control all of the various needed speed selection modes only using pin AN0 (pin 22)

    I will ask the team and follow up if I have a different answer

    Best,

    Alon