Part Number: DP83826I
Team,
my customer has a question about the sequence of the AVDD3V3 and VDDIO voltages. They are powering the device up in the following sequence and wanted to undertstand if this is ok:
- VDDIO starts with 1.8V.
- A few milliseconds after that, AVDD3V3 starts with 2.5V
- Some hundret milliseconds later, AVDD3V3 is going to 3.3V
During this time, the PHY is held in reset by a GPIO with pull-down. They are planning to release the reset after all voltages are initialized correctly.
Best regards