Hello expert,
Customer is asking if we can implement below application. Could you check if below block is workable? Thanks a lot!
Best regards,
Ann Lien
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello expert,
Customer is asking if we can implement below application. Could you check if below block is workable? Thanks a lot!
Best regards,
Ann Lien
Hi Ann,
Thanks for reaching out. Yes, in backward-compatible mode, the DS90UB949 supports up to 720p resolutions with 24-bit color depth over a single differential link. Also, the DS90UB928 can support High definition (720p) Video resolution.
Note – The DS90UB949 is backward-compatible to the UB928 for PCLK ranging from 25 MHz to 85 MHz. Also, backward compatibility does not need to be enabled. When the DS90UB949 is paired with a backward compatible device, the serializer will auto-detect to 1-lane FPD-Link III on the primary channel (DOUT0±).
Also, the PCLK of the transmitted video should less than 85 MHz to be supported by a single FPD-Link channel. Make sure your active video + blanking resolution meets this PCLK requirement
Regards,
Fadi A.