Part Number: DP83822I
Hello,
I'm encountering an intermittent occurrence with our devices, where the device never establishes a link when an ethernet cable is connected.
I've tested all the cables involved with a network cable tester and that all seems good.
This is the debug output of the DP832822 registers before and after the ethernet cable is connected (same value in both cases):
00: 0x300001: 0x784902: 0x200003: 0xA24004: 0x00A105: 0x000006: 0x000407: 0x200108: 0x000009: 0x000010: 0x010011: 0x100012: 0x000013: 0x000014: 0x000015: 0x000016: 0x400217: 0x000318: 0x002019: 0x080020: 0x000021: 0x000022: 0x010023: 0x004124: 0x048025: 0x800126: 0x000027: 0x007D28: 0x05EE29: 0x000030: 0x010231: 0x000016: 0x0002
16: 0x400219: 0x000019: 0x0800