Part Number: TCA9548A
Other Parts Discussed in Thread: LDC1614
Hello there,
I am facing problems to establish I2C communication between MCU (master) and TCA9548A. (Not response
on default I2C address 0x70, but A0-A2 grounded).
For further test setup simplicity, can I neglect all channel considerations like pullup resistors dedicated to the individual channels etc?
At current debug stage, I only want to establish I2C comm between the master and a single slave device, and reading and writing the status register.
Once that is working, I will look into channel usage.
Obviously, I have pullup resistors in place (4.7K) for this simplified test setup.
Regards,
Jo