Hi,
We're using the devices mounted on our PCBs for over 2 years now, and having reasonable performance so far without any functional problems.
[Our design is based on synchronous mode.]
Recently we initiated automotive environmental testing, and got the following problem after unpowered thermal shock test on some of the PCBs:
1. No link with the receiver board (954).
2. when debug from the serializer side LINK_DET is either 0 or unstable.
3. The full GENERAL_STATUS register is found in one of the following values 0x00, 0x01, 0x20, 0x21 (not clear from datasheet what is bit [5]).
4. the power, PDB, boot straps are ok.
The PCBs were fine before the test, and the failures are clearly related to the physical stress, however we do not observe any visible/xray problem on the PCB or device.
Can you advice what could lead to such a problem?
should we look for a specific solder joint? trace?
known weakness of the device?
Is there any clue from bit [5] value?
thanks,
amotz
thanks,
amotz