We are trying to implement a function to select one from multiple RS422 specification trigger signals (pulse signals of several hundred uss) and a function to distribute the selected one to multiple.
The parts used are (IC-A) 422 receiver: AM26C32CD and (IC-B) 422 driver: AM26C31MDREP.
-Use three of (IC-A) to convert each of the three RS422-spec trigger signals into a single-ended signal.
-Integrate the three outputs (single end) of (IC-A) into one in a pattern, and connect them to the eight inputs of two (IC-B).
-Control the G / G bar signal of ① and select only one trigger signal.
-The selected trigger signal is output as a 422 signal branched into 8 systems.
I would like to confirm the points of concern when designing the circuit.
Q1. Is it possible to branch the signal into 8 branches in terms of the output capacity of (IC-A) and the input capacity of (IC-B)?
Q2. Is pull-up or pull-down processing necessary for the output of (IC-A)?
Q3. Is it necessary to provide damping in the wiring between (IC-A) and (IC-B)? If so, what are the wiring and damping resistance placement requirements?
Q4. Are there any other points to be aware of or concerns? Thank you for your cooperation.