Part Number: SN65HVD485E
Hi
The fail safe of the SN65HVD485E may not work on our customer's system.
There is no external bias resistor for fail safe.
The customer's process inspection is as follows.
Failure is caused by sending an unintended Start Bit during Bus idle before sending a command (TX).
Normally, the receiver in the bus idle state should output Hi, but since VA-VB (differential bus voltage) is -0.8V, it seems to output Low.
Why is internal bias not enabled?
The device failure analysis result was Pass.
Best regards,
Hiroshi