Part Number: DS90UH947-Q1
Hi Expert ,
Several questions about 947 and 948,
- 947 oLDI interface have 8 data lane and 1 clock lane while 948 have 8 data lanes and 2 clock lane, why the two OLDI interface is different?
For 947 side, the standard SOC oldi interface should contain 1 clock lane and 4 data lane. How if the SOC can not support 1 clock lane with 8 data lanes?
2. clock limit
the highest frequency of 947 clock limit is 96MHz @ single lance and 170MHz @ dual lane while the highest frequency of 948 clock limit is 96MHz @ single lance and 192MHz @ dual lane .
Why the 947 dual lane frequency is lower than 948 while single lane the same?
Thanks
Best regards,
David