Part Number: PCA9546A
A few questions about reset:
- The data sheet 8.4.1 states "The /RESET input must be connected to VCC through a pull-up resistor". I have a design where the /RESET line is driven from a TTL output from an MCU. The MCU and PCA9546A are both powered from the same VCC = +3.3V. The MCU powers up with outputs floating until firmware enables totem pole so the/RESET line is not pulled or driven until after VCC rises to 3.3V on powerup. What problems might result from this?
- The data sheet 8.4.2 states "Thereafter, VCC must be lowered below VPOR to reset the device". Is asserting /RESET different than Power_On_Reset and how so?
Thanks
Phil