Part Number: TCAN1167-Q1
In the circuit described in the data sheet, a limiting resistor of 33kΩ is connected to the WAKE terminal, and a capacitor of 0.1nF is connected in parallel with the SW. Could you tell us the role of these two points? I want to reduce the number of parts as much as possible, so I want to make it unmounted (resistor is short, capacitor is open), but I want to check if it is possible, so please tell me the role.