Dear technical team,
we are using the DP83TG720 PHY on one of our electronics and want to connect it to an external SPE to 1000Base-T converter also designed by ourselves in a space constrained scenario. We have observed severe performance issues (1MB/s max datarate) if the PHY registers are not configured by the Linux driver for both master and slave side. If the registers are set, the datarate is much better in a range of 85MB/s which is sufficient for our applications.
1. is it mandatory to configure the PHY so that it is most robust in a slave and master scenario?
2. Is there a revision planned that inherits the driver register settings without need of direct register access or is there a kind of workaround?
Thanks a lot and have a nice day,
Bernd