Part Number: DP83869EVM
Other Parts Discussed in Thread: DP83869
Dear team,
I see that DP83869EMRGZT in the BOM of DP83869EVM.
I found several e2e posts about this topic but the answer is different.
I think the big difference is VDD1P1, 1.1V and 1.0V.
In addition, 1.0V cannot be used for -HM because according to D/S 1.1V +/-10% is needed.
My customer evaluated and tries to adopt it but they must use 1.0V as same as EVM because they also use 1.0V for FPGA.
Can they buy DP83869EMRGZT as production?
Or do they have to use 1.1V with -HM?
Best regards,
Yuto