Part Number: DS90UH949-Q1EVM
Hello,
We have programmed an EEPROM with all EDID data.
The EEPROM is pluggen in U3. MODE_0 is 5 and MODE_1 is 1.
HDMI is already connected before powe-up the DS90Ux949EVM. After power-up the DS90Ux949EVM , we can see the image correctly for abaut 1 second and then image the image disapear.
If we power-up the DS90Ux949EVM and after that we connect the HDMI we do not see any image.
In both cases, if we press the S4 PDB then we can seen the image and it is stable and does not disapear.
What can we do to initialize correctly the image with the EDID from the local EEPROM? Can we send a I2C command?
Many thanks, Jose