Part Number: TVS3300
Hi,
This post is regarding SLVAE37 app note, which references TVS3300.
Towards the bottom of page 6, it mentions RDYN of SMAJ33A to be 884mOhm and RDYN of SMBJ33A to be 0.504Ohms. I looked in the datasheets for these parts and did not find this number. I also tried dividing VCLAMP
with IPP and did not get these numbers.
For TVS3300, on page 6 of its datasheet, RDYN is listed as 60mOhm max. Test Conditions column says this was calculated from VCLAMP at 15A and 30A surge current levels. I was not able to calculate this RDYN either.
Can someone please show me how RDYN was calculated for SMAJ33A, SMBJ33A, and TVS3300?
(All datasheets and app note are attached.)