Part Number: DS90UB936-Q1
Hi team,
As the shortage of UB954, can UB936 replace UB954 without any change? The ser is UB933, 1920*1080*30. Thanks!
Thanks!
Jiawei
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB936-Q1
Hi team,
As the shortage of UB954, can UB936 replace UB954 without any change? The ser is UB933, 1920*1080*30. Thanks!
Thanks!
Jiawei
Hello Jiawei,
You are correct, the UB954 can be replaced with the UB936 with no changes needed, only thing to keep in mind is that while the DS90UB954 can accept up to 4.16 Gbps from a single camera the DS90UB936 can only accept up to 3 Gbps from a single camera.
Regards,
Joshua