Part Number: TCAN4550
Other Parts Discussed in Thread: ISOW1044,
I have a client that requires galvanic isolation for their CAN bus physical interface, requiring an external transceiver such as the ISOW1044. Is it an officially supported configuration to use test mode with mode/pin register bit 21=1 and bit 0=1 to map the internal RXD/TXD signals externally via GPIO1/GPO2 (as illustrated in the data sheet Fig. 29) to accomplish this?
Thanks in advance.
Tom Nelson
Granite Computer Sciences, LLC