Part Number: TFP410
Hi team,
My customer convert the input 24bit RGB signal to DVI by TFP410. The consistency test of TFP410 is failed. See the differential signal D0/1/2 in the picture. It can't work when we try to change the differential signal amplitude by adjusting the resistance of TFADJ pin. The length of the DVI differential signal from the pins of the TFP410 to the connector is about 3300 mils, and the internal length difference is within 30 mils.
Do you have any suggestion to optimize the signal ?

Thanks a lot
Matthew