Part Number: TCA9548A-Q1
Other Parts Discussed in Thread: TCA9548A
HI,
1. We are going to use TCA9548A-Q1 to expand the I2C interface. If the expanded 8-way I2C interface is connected to different I2C address devices, can only one of the expanded interfaces SCX/SDX be connected to the SCL/SDA main interface at a time?Or 8 expansion I2C can be connected to SCL/SDA interface at the same time?
2. What are the advantages of TCA9548A-Q1 compared with analog switches?
3. A0/A1/A2 is used to set the I2C address of TCA9548A-Q1, right?
4. When communicating with the I2C device attached to the SCX/SDX interface, does the main SCL/SDA interface need to transmit two I2C addresses? First send the I2C address of TCA9548A-Q1 set by A0/A1/A2, and then send the I2C address of the device that connect to SCX/SAX?