This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Which parts do you recommend for converting between 100BASE-T and 100BASE-T1 similar to the DP83TC811EVM board? The evaluation board uses DP83TC811 and DP83822 but there are also other alternatives. Maybee DP83TC813 and DP83826.
Do I need to configure the devices with MDIO or may it work with default settings and hardware strappings. Then I could skip a microcontroller.
Is there any device (-T and -T1) that can handle both 100MB/s and 1000MB/s that allows to design a converter for both speeds?
Hi Bo,
A media converter can be created between any 2 PHYs connected back to back through MAC interface. For 100Base-T to 100Base-T1, the design would be as follows: PHY1 set to 100Base-T to RMII mode, PHY 2 set to RMII to 100BASE-T1 mode. The same idea works for 1000Base-T to 1000Base-T1, using RGMII as the MAC interface.
It is theoretically possible to make such a design work with default settings and hardware strappings, but it is strongly recommended to include a microcontroller to load optimized configurations and debug.
We currently do not offer any automotive PHYs that support multiple speeds unfortunately.
Thanks,
David