Part Number: TLK2711-SP
The TLK2711's reference circuit is defined as a ferrite bead 5ohm@100MHz.
Is there any problem with using 30ohm@100MHz or 600ohm@100MHz ferrite bead?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLK2711-SP
The TLK2711's reference circuit is defined as a ferrite bead 5ohm@100MHz.
Is there any problem with using 30ohm@100MHz or 600ohm@100MHz ferrite bead?
Hi,
I would not recommend using 600 Ohm @ 100 MHz since this would likely incur non-trivial impedance at frequencies lower than 100 MHz. 30 Ohm @ 100 MHz would probably work fine, but please keep in mind that this is not something we have validated.
Thanks,
Drew