Part Number: TLK2711-SP
As I know TXCLK maximum jitter of TLK2711 is 40ps.
I use RTG4 PLL clock(from 50MHz to 80MHz) for TLK2711's TXCLK.
Would it be okay?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLK2711-SP
As I know TXCLK maximum jitter of TLK2711 is 40ps.
I use RTG4 PLL clock(from 50MHz to 80MHz) for TLK2711's TXCLK.
Would it be okay?
Hi,
I assume you would be using the RTG4 PLL clock at 80 MHz? What is the jitter and logic levels of this clock?
Thanks,
Drew
The RTG4 receives 50 MHz of the oscillator. And RTG4 generates 80MHz using PLL and outputs it to TXCLK of TLK2711.
Logic level is LVCMOS 2.5V.
Please refer to the below data of RTG4 PLL jitter.
Hi Dean,
The first part of the jitter calculation means that the RTG4 clock would not be suitable since the maximum jitter for TLK2711 TXCLK is 40 ps.
"Max(80 ps, 2% * (1/fin) )"
Thanks,
Drew