Part Number: DS100BR410
Other Parts Discussed in Thread: DS50PCI401, DS50PCI402
We are using the DS100BR410 for a cabled PCI express (gen1) application as replacement of the DS50EV401SQ/NOPB (which is EOL).
we run into the issue that the link is not established.
when measuring on the input of the DS100BR410 (IN_0+/IN_0-) we see the beacon pulse of PCI express but the SD0 output remains low and no signal is measured on the output of the DS100BR410 (OUT_0+/OUT_0-).
the beacon pulse measured with a single ended probe has an DC offset off approx 1.4V.
when we pulse the IN_0+ or IN_0- to GND the PCI express link is established and everything seen to work fine.
what would cause the issue that the beacon pulse is not detected by the DS100BR410?
Thanks
Jeroen