Part Number: TPS65982
Other Parts Discussed in Thread: TPS65981
Hi,
We use TPS65982 with TUSB546AI for USB-C DP-Alt mode as a host. The unit is working fine with the TI provided firmware (TPS65982.bin) file. I need to generate a document, which includes the source file and verify the binary file. From TI Application Customization Tool, I imported the binary file (by selecting "Change file" button) and then saved the binary file. An error stated the file too big. It seems the configuration size (see attached image below) is too big (4294967295 bytes). If this is the problem, can I change the Configuration size? I can provide the binary if needed. Also, is there another war way to generate the source file?
FYI, I have tried using "default.bin" file from the application and also "Import Setting from Device", both binary files did not match the provided TPS65982.bin file.
Thank you in Advance