Part Number: DS90UB949-Q1EVM
Other Parts Discussed in Thread: ALP
Hello all,
I am trying to interface the DS90UB949-Q1EVM board using an MCU through I2C. I am also connecting the ALP tool to see the registers of SER and DESER. But the issue is, when I am connecting the ALP tool to the SER, the clock lines are observed over the J20 header of SCL pins, as well as the SDA pin, which is also having some transitions between high to low and vice-versa. It means something is already doing I2C transfers on the J20 header. But, as the schematic https://www.ti.com/lit/ug/snlu169/snlu169.pdf?ts=1655049603601&ref_url=https%253A%252F%252Fwww.ti.com%252Ftool%252FDS90UB949-Q1EVM,

As seen in the schematic, attached above, I am not seeing any IC connected over SDA and SCL lines, that are initiating the I2C transactions. So please let me know what is the source of the I2C information.
On the J20 header, I have to connect an external MCU EVK. Will this already existing I2C communication affect the new I2C connection with external MCU EVK?