Part Number: TUSB2046B
I made a USB hub device using the TUSB2046B.
However, the device works normally when three USB devices are connected, but when the fourth device is connected, all connected devices are disconnected and reconnected again and again.
The devices we connected are all 4 keyboards, under USB 2.0, and the speed is Full-Speed.
first equipment

second equipment

The 3rd and 4th devices connect 2 keyboards of the same model