Part Number: THVD1505
Other Parts Discussed in Thread: THVD1500, THVD1429, THVD1510
Team,
just to be sure:
THVD1500 can be directly replaced by THVD1505 on an existing PCB designed for THVD1500. Correct?
It is 100% backward compatible. Correct?
In fact all THVD1xxx half duplex ICs (like THVD1510/20/52, THVD1429/39/50, .etc) can be used in place of the THVD1500. Correct?
Or are there some potential issues to use higher speed THVD1xxx for lower speed?
Thanks in advance,
A.