Part Number: DS90CR286A
Other Parts Discussed in Thread: DS90CR216A
Hello forum members, I was hoping to use this chip as a straight 1:7 receiver on each channel, but the input to output mapping doesn't seem to match up in the way I expected. I would have thought that the sequential RxOut pattern would continue in much the same way as in it's DS90CR216A 3 channel counterpart.
I figured each channel's sequence would map as:
[ RxOut6 RxOut5 RxOut4 RxOut3 RxOut2 RxOut1 RxOut0 ] for each channel such as in the DS90CR216A.
However the outputs observed in data sheet shows:
[ RxOut7 RxOut6 RxOut4 RxOut3 RxOut2 RxOut1 RxOut0 ] and some similar mappings for the other channels as well.
Is it possible to use this device for arbitrary data readouts of a serialized LVDS line? My serialized signal does not include HSYNC, VSYNC, or DE within the data, it only includes arbitrary values from an image sensor (all the frame start/stop and data types are baked into the individual pixels themselves, not represented as their own bit). Does this strobe just act as a simple 1:7 de-serializer with a non-sequential mapping scheme?
Also, I believe there is an error in the data sheet on pages 19-20, if any TI employees here see this, they might be interested in correcting it.
Table 2:
The mapping of RxIN0 shows only 6 positions mapped to it when TxIN7 should be included in that table section as seen from the timing diagram in Figure 6. I believe it most likely spilled over into RxIN1's section on the first entry. RxIN1 has 8 mappings instead of 7 like them rest of them, so this seems plausible.
Table 3:
This table has the same issue with RxIN0 as stated above for Table 2.