Part Number: TIOS101
Hi Team,
I have a question about TIOS101 abso max ratings and driving inductive loads.
TIOS101 CQ pin abso max is ±65V(transient pulse width < 100us for VCC and OUT).
"9.2.2.3 Driving Inductive Loads" mentions a significant amount of inductive kick back is clamped internally at about ±75V.
How do we consider the relationship between ±65V and ±75V?
If we use inductive load and its significant amount of inductive kick back exceeds ±65V, TIOS101 has internal clamp diode so it is no problem even though it violates ±65V abso max?
±75V is not described in abso max spec so I'm not sure ±75V is just for protection.
±75V is just protection so we have to follow abso max spec or we can say that device can support up to ±75V under driving inductive loads?

Regards,
Kai