Part Number: THVD8000
Other Parts Discussed in Thread: THS6222
Hello,
I recently bought 3 EVM of the THVD8000 to test the component in order to implement it on our products.
The first tests without connecting to the GND of the power supply to the earth went well, but when I tried to connect the GND to the earth it obviously stopped the communication between the modules.
Here is the model I tried :

And I have seen this thread that represent a similar implementation (24V DC power supply and data, up to 64 nodes, up to 80 meters, and the maximum data rate possible) that I would like to do with the only difference that the GND of the power supply must be connected to earth.
Also I saw on the answer that it was possible to connect the GND of the power supply to the earth but the communication would be only with one wire.
Do you have more documentation or information about how to communicate with the GND connected to the earth to and how should I configure the evaluation module please?
Have a good day,
Cordially.
Hugo