Hello Team,
We would like to have the following setup
Single DSI Input to DS90UB941 and two displays as below:
SoC -> DSI -> DS90UB941->DS90UB948->1280x800 TFT
->DS90UB948->800x480 (DLP) Displays.
As we know 941 can support splitter mode and it has both symmetric and asymmetric method in splitter mode.
For the above scenario which mode you would suggest and is it feasible to implement a solution with the above resolutions.
Please help to suggest.
Thanks,
Sundar

Please find the timing parameters of 2 displays respectively.