Part Number: TRS213
Other Parts Discussed in Thread: MAX213, MAX3243E, TRS3243E, TRS3243, MAX3243
Hi Expert,
May I know the difference between MAX3243EIDBR & TRS213IDBR?
Which one has the better ESD protection?
BR,
Aaron Chen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The TRS213 is identical with the MAX213.
The TRS3243E is mostly identical with the MAX3243E.
The TRS3243E/MAX3243E are TRS3243/MAX3243 with better ESD protection.
The '213 and '3243 devices have a different number of channels, a different pinout, a different maximum speed, and different supply voltage support.
What features do you actually need?