RX_D3 pin must be pull down with 2kΩ, then can enter MODE 1. If RX_D3 is open, RX_D3 is strapped to MODE 4. Since the datasheet shows that the RX_D3 is strapped to MODE 1 with RX_D3 open, I like to know why this phenomenon occurs. My Schematic is show blow, the DP83TG720RWRHATQ1 is the chip replace with DP83TC811RWRNDTQ1.
.