Hello,
My customer would like to connect TUSB1046A-DCI to either USB3.1(Gen2) or displayport via USB typ-C cable. Depending on whether the TypC cable is connected to USB3.1(Gen2) device or displayport device, RX1P/N and RX2P/N pins would be either Tx or Rx. In this case, should RX1P/N and RX2P/N pins have ac-coupling caps like TX1P/N and TX2P/N pins in the Figure 28 of the datasheet?
Best regards,
K.Hirano