Part Number: TS3DV520
hi i m using thi multiplexer there is thermal pad (pin 57) should i connect the pad to other pins like ground?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ground or floating; see [FAQ] Where do I connect the thermal pad of the logic QFN devices?
Hi,
For TS3DV520, please solder thermal pad to the board ground for better thermal and mechanic performance.
Please also use the stencil pattern as shown below and solder coverage must be at least 68%.

Thanks
David