This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DP159: DEV_FUNC_MODE function

Part Number: SN65DP159

Hi team

What is the difference for these two modes? And how to configure this for HDMI application? 

  • Hi,

    Automatic retimer for HDMI2.0 -> Based on the TMDS_CLOCK_RATIO_STATUS bit. Will be in redriver mode when TMDS_CLOCK_RATIO_STATUS is 0 and retimer mode when TMDS_CLOCK_RATIO_STATUS is 1. 

    Retimer mode across full range 250 Mbps to 6-Gbps -> Retimer only across the entire data rate. 

    For now I would recommend leaving it in its default setting unless there is a specific reason to change it.

    Thanks

    David