Part Number: DS100KR800
Hi team
My customer is using DS100KR800 for FPGA SERDES port between two boards and they want to know if DS100KR800 is supporting Bypass mode?
(FPGA SERDES -> DS100KR800#1) -> 2m 10G cable -> (DS100KR800#2 -> FPGA SERDES)
The customer found the eye diagram is better if DS100KR800 EQ and PE both are configured to 0dB and any adjustment of EQ and PE made the quality of eye diagram worse, but the quality of eye diagram is not so good even under 0dB configuration. Hence the customer wants to know:
- If DS100KR800 is supporting bypass mode? The customer wants to double check if DS100KR800 is necessary for their application.
- When EQ and PE both are configured to 0dB, is is okay to see DS100KR800 is in bypass mode? What processing is performed on the signal in this mode?
- Considering there is only a 2m cable between two boards, hence if the loss between two DS100KR800 is small, will using DS100KR800 cause the signal quality to deteriorate?